Silent Installation

CSense supports a silent installation from the command line. An INI file is used to configure the installation options and is specified as a command line argument to the installer.
The INI file must be in the following format:

[SetupValues]
<Parameter1>=<value1>
<Parameter2>=<value2>

Silent install is run from an Administrator command line using the following format:

start /wait Setup.exe “/S:<path to .ini file>”

The INI file supports the following parameters:

Parameter Name

Default

Description

%ExpressInstall%

1

“1” for Express installation or “0” for Advanced Installation.

%AppFolder%

C:\Program Files (x86)\Proficy\Proficy CSense

Installation Folder.

%CacheFolder%

C:\Proficy CSense Cache

Cache Folder.

%DatabaseServer%

(local)

Location of the SQL Database Server that must be used. Ignored when %ExpressInstall% is “1”.

%InstallDataServer%

1

“1” if the CSense Data Server component must be installed or “0” if the CSense Data Server must not be installed.
Ignored when %ExpressInstall% is “1”.

%InstallApplicationServer%

1

“1” If the CSense Application Server must be installed or “0” if the CSense Application Server must not be installed.
Ignored when %ExpressInstall% is “1”.

%CustomServicesAccount%

0

“1” If the CSense Services must be installed to a custom account. If set to “0” then the Local System Account is used for services.
Ignored when %ExpressInstall% is “1”.

%ServicesUser%

 

The account that must be used for services if the %CustomServicesAccount% is set to “1”.
Ignored when %ExpressInstall% is “1”

%ServicesPassword%

 

The password for the %ServicesUser% if the %CustomServicesAccount% is set to “1”.
Ignored when %ExpressInstall% is “1”.

If the %ExpressInstall% parameter is set to “1” then only the following parameters will be respected and the rest of the parameters from the INI file will be ignored, and their default values as specified will be used:

  • %AppFolder%

  • %CacheFolder%

If the %ExpressInstall% parameter is set to “0” and %InstallDataServer% is “1” then the following parameters will be used:

  • %DatabaseServer%

If the %ExpressInstall% parameter is set to “0” and %InstallApplicationServer% is “1” then the following parameters will be used:

  • %AppFolder%

  • %CacheFolder%

  • %DatabaseServer%

  • %CustomServicesAccount%

  • %ServicesUser% (if %CustomServicesAccount% is “1”)

  • %ServicesPassword% (if %CustomServicesAccount% is “1”)

Any parameter not specified or left empty will use the default value.

When specifying a %CustomServicesAccount% and the user is a domain user, the domain credentials information must be specified in either User Principal Name (UPN) format or Down-Level Logon Name format.

Example of Express Install into custom locations

.ini file name: SilentInstallExpress.ini

.ini file contents:

[SetupValues]

%ExpressInstall%=1

%AppFolder%=C:\CSense Install

%CacheFolder%=C:\CSense Cache

Command

start /wait Setup.exe “/S:C:\SilentInstallExpress.ini”

Example of Advanced Install (installing only the CSense Data Server to the local SQL Database Server)

.ini file name: SilentInstallDataServer.ini

.ini file contents:

[SetupValues]

%ExpressInstall%=0

%InstallDataServer%=1

%InstallApplicationServer%=0

Command

start /wait Setup.exe “/S:C:\DataServer.ini”


Related topics:

  

CSense 2023- Last updated: June 24,2025